Technical FAQs

Ask a Question

What is the difference between the LIL and the LCL circuit breakers?

The difference between these two breakers is the interrupting rating. The LCL breaker is the lower of the two, with a rating of 100K at 240V, 65K at 480V, and 35K at 600V. The LIL breaker has a rating of 200K at 240V and 480V, and 100K at 600V.


CTA-ID : 2025286
Was this helpful?
What can we do to improve the information ?