Technical FAQs

Ask a Question

What is the magnetic trip level of a QOB115HM?

The QO115HM high magnetic breaker is calibrated so that the magnetic trip could occur between 315 A and 525 A.


CTA-ID : 2025075
Was this helpful?
What can we do to improve the information ?