Technical FAQs

Ask a Question

How do you reset the M6C or M2C latching contacts after an alarm?

The M2C can be set up for latching or non-latching contacts. If set for latching, you have to reset in the M2C/M6C menu of the ``wrench`` key on the face of the trip unit. The reset button on the trip unit will reset the trip unit indication but will not reset the M2C.

CTA-ID : 2024898
Was this helpful?
What can we do to improve the information ?