Technical FAQs

Ask a Question

Does the Powerpact P frame breaker come with the studs for bus connection?

Issue:
Bus connection with Lugs - lugs breaker ?

Product Line:
Molded Case Breakers

Environment:
Powerpact P

Cause:
Installation

Resolution:
 The bus connection kit S33928 comes installed on P frame breakers with an F in the third position  ( ie. PGF36120 ).


CTA-ID : 2024896
Was this helpful?
What can we do to improve the information ?