Technical FAQs

Ask a Question

Is the QO24L60NRNM load center suitable for use as service equipment?

Issue:
Product design features

Product Line:
QO load centers

Environment:
Service Entrance rating

Cause:
Application

Resolution:
Yes. The following statement is provided on the device directory label, located on the front of the interior trim: "Suitable for use as service equipment. When used as service equipment, install jumper wire between panel neutral and equipment ground bar in accordance with applicable codes".


 
Was this helpful?
What can we do to improve the information ?