Technical FAQs

Ask a Question

How do I join two pieces RWT06S18S wall duct together? Is any additional hardware required?

On the RWT type wall duct, couplers are included with the units. There is no additional hardware needed.


CTA-ID : 2025272
Was this helpful?
What can we do to improve the information ?