Technical FAQs

Ask a Question

Can a QC816F150C be used for an overhead or underground feed application?<br /><br /><br />

Yes, this device is suitable for either overhead or underground feed applications.





CTA-ID : 2024874
Was this helpful?
What can we do to improve the information ?