Technical FAQs

Ask a Question

What does the suffix TO25, TO50, and TO100 on a XPSAT indicate?

These indicate fixed timing ranges on the timed output contacts, TO25 is a fixed 25sec delay, TO50 is a fixed 50sec delay, and TO100 is a fixed 100sec delay. Standard XPSAT`s have adjustable timing delay on the timed contacts.


CTA-ID : 2025262
Was this helpful?
What can we do to improve the information ?