Technical FAQs

Ask a Question

What is the cable with straight connector for a sensor with K suffix such as XS1M18MA230K ?<br /><br />Corrected Inquiry and Response grammar and added Key Words. Added further description and info on U20 designator.

Connector is a 3 pin female AC/DC Micro connector. This is reserved for AC applications and can be identified by the double key and 1/2``-20 thread. On newer Telemecanique sensors, the ``K` designator is changed to ``U20`` which is dimensionally and electrically identical.
XSZCK111Y Yellow PVC 2 meters
XSZCK112Y Yellow PVC 5 meters
XSZCK113Y Yellow PVC 10 meters
XZCP1865L2 Black PUR 2 meters
XZCP1865L5 Black PUR 5 meters
XZCP1865L10 Black PUR 10 meters


CTA-ID : 2025257
Was this helpful?
What can we do to improve the information ?