Technical FAQs

Ask a Question

What is the difference between a NHL361200 and a MHL361200 ?

The 12``w x 20``h NHL 361200 has lugs for 4 350-750 kcmil , is 480v max 50 k AIR rated and is obsolete. The newer 9``w x 14``H MHL has terminations for 4 #1/0-350 kcmil and is rated 600 V 65 k AIR max .

CTA-ID : 2025256
Was this helpful?
What can we do to improve the information ?