Technical FAQs

Ask a Question

Looking for how to defeat the long time memory on a Digitrip 810 trip unit when performing secondary injection testing.

Under the rating plug, remove the jumper and reinsert into the top two holes. This makes the long term memory inactive. Or customer to start a self test and canx the self test prior to the breaker tripping. This will also reset the thermal memory. Assistance from Field Services Gary Dunn.

CTA-ID : 2035343
Was this helpful?
What can we do to improve the information ?