Technical FAQs

Ask a Question

What is the part number of the replacement diagnostic cables in Surgelogic devices?

Product Line:  
Surge Protective Devices (SPDs)

Environment:
Maintenance

Cause:
Replacement parts

Resolution:
TVS19PCK (Three 19 in. (48.3 cm) cables)
TVS36PCK (Three 36 in. (91.4 cm) cables) Typically found in EMA/EMBA, I-lINE, NQOD, NF, Federal Pioneer & Busway.
TVS60PCK (Three 60 in. (152.4 cm) cables) Typically found in QMB, QED, & MCC`s.
TVS192PCK (Three 192 in. (487.7 cm) cables) Typically found in PC3/PZ4.
Was this helpful?
What can we do to improve the information ?