Technical FAQs

Ask a Question

TVS4EMA24AIC, Need confirmation that the unit must be replaced if the handle has broken off.

Entire unit DOES NOT need replaced. Handle = Part# 6600-0052 or Shaft = Part# 6600-0053 or Switch = 6600-0055
Contact TVSSTAG 800-577-7353
e-Mail for replacement.

CTA-ID : 2025066
Was this helpful?
What can we do to improve the information ?