Technical FAQs

Ask a Question

Is the Universal Test Set UTS3 forward/backward compatible with the Full Function Test Kit, FFTK and the Hand Held Test Kit HHTK, in regard to testing Micrologic Series B, and Micrologic 3.0, 5.0, 6.0 A/P/H trip units?

No. The UTS3 will test the Series B. The FFTK and the HHTK will test the 3.0, 5.0, 6.0 A/P/H trip units.


CTA-ID : 2024627
Was this helpful?
What can we do to improve the information ?