Technical FAQs

Ask a Question

How many electrical accessories can be put into an LA or LH circuit breaker?

You can put 3 accessories in an LA, LH, or Q4 breaker if one is a bell-alarm. If there is no bell-alarm, you can install two accessories.
If the breaker has a bell-alarm (factory-installed only), the right pole accessory must also be factory-installed.


CTA-ID : 2025249
Was this helpful?
What can we do to improve the information ?