Technical FAQs

Ask a Question

What can be done to solve nuisance tripping with a QO breaker on a microwave circuit ?

Use a QO115HM or QO120HM for QO load centers, or HOM115HM or HOM120HM for HOMELINE load centers. The HM suffix provides a breaker with a higher inrush withstand capability to allow the Microwave to function .

CTA-ID : 2025244
Was this helpful?
What can we do to improve the information ?