Technical FAQs

Ask a Question

Does an XS2M30MA230K come with a cable?<br /><br />Changed Response to correctly read ``straight connector`` rather than ``90 degree head ``

No, It has a AC/DC micro style quick disconnect connector and no cable. The suffix K or U20 codes for this type of connector. For a list of cables see sensors catalog 9006CT0101 page 530. Example cable would be the XSZCK101Y (1.8 Meter) with straight connector .


CTA-ID : 2025242
Was this helpful?
What can we do to improve the information ?