Technical FAQs

Ask a Question

Will a 6.0P trip unit be lit when it has voltage on its load side stabs?

Yes, P and H trip units should be lit when the breaker has voltage on the load stabs.



CTA-ID : 2025239
Was this helpful?
What can we do to improve the information ?