Technical FAQs

Ask a Question

I have a central vacuum and it trips the HOM circuit breaker when I turn it on. Is there a problem with the central vacuum?

Most likely, the central vacuum does not have a problem, but we recommend that you have a qualified technician verify that the central vacuum system is operating appropriately. You may need to have the Central vacuum wired to a separate circuit that will handle the Central vacuum high inrush and running current


CTA-ID : 2025055
Was this helpful?
What can we do to improve the information ?