Technical FAQs

Ask a Question

I have a central vacuum and it trips the HOM circuit breaker when I turn it on. Is there a problem with the Branch Circuit Breaker?

Central vacuum motors have a high inrush and large running currents that can cause the Circuit breaker to trip. You may need to have the Central vacuum wired to a separate circuit that will handle the Central vacuum high inrush and running current


CTA-ID : 2025053
Was this helpful?
What can we do to improve the information ?