Technical FAQs

Ask a Question

Can a SC12L200F be used for an overhead or underground feed application?

Yes, this device is suitable for either overhead or underground feed applications. However, for an overhead application, a Tunnel Kit must be field installed. Order SCTK20 separately.


CTA-ID : 2024852
Was this helpful?
What can we do to improve the information ?