Technical FAQs

Ask a Question

Can a SO1020M100S be used for an overhead or underground feed application?<br /><br /><br />

No, this device is suitable for an overhead feed application only.





CTA-ID : 2024846
Was this helpful?
What can we do to improve the information ?