Technical FAQs

Ask a Question

Can a SC2040M200S be used for an overhead or underground feed application?<br /><br /><br />

Yes, this device is suitable for either overhead or underground feed applications. However, this device is approved for underground service only with Arizona Public Service (APS) or Salt River Project (SRP) utility companies.

CTA-ID : 2024842
Was this helpful?
What can we do to improve the information ?