Technical FAQs

Ask a Question

When using a EZM Main Tap box, for a EZM 3 Phase IN-3 Phase OUT Commercial Line up, can 3 Phase IN-1 Phase OUT Branch Devices be used?

EZM application

Product Line:
EZM Metering

Installation of Branch metering devices

EZM Line up installation

Yes, For a 3phase incoming EZM line up, BOTH 3phase OUT and 1Phase OUT EZM branch Devices can be used in the same line-up.  Depending on the size of the Main(Max. Ampere rating), will determine which branch devices must be used. The requirements for mounting the Main and branch devices are located in the instructions that come with ALL the EZM devices and can be found on digest page 2-8, lower left corner of the page, the 5 bullets under the heading "Main Devices".

CTA-ID : 2025229
Was this helpful?
What can we do to improve the information ?