Technical FAQs

Ask a Question

Why can`t I pick a Utility Meter Section connecting to an HVL/cc for NEMA 3R in the medium voltage metal enclosed product selector?<br />

The outdoor enclosures for HVL/cc and HVL are not the same. The rooflines do not match up and there are no standard assemblies at this time. The HVL type Utility Meter Section should be entered as a separate line item. Add a 24`` Outgoing Section to the Meter Section for pricing and a 3`` collar for roofline conflicts. If it is a Cold Sequence Meter Section, then transitons will be required on both sides of the Meter Section.



CTA-ID : 2015430
Was this helpful?
What can we do to improve the information ?