Technical FAQs

Ask a Question

Does Square D offer a 600 Amp, 600V AC, NEMA 4X, Stainless Steel Double Throw Safety Switch?

Issue:
Product availability

Product Line:
Double throw safety switches

Environment:
Maximum amperage switch

Cause:
Application

Resolution:
No, The maximum 600Vac NEMA 4X Stainless Steel Double Throw Safety Switch Square D offers is 400 Amp. SEE CURRENT DIGEST FOR CATALOG NUMBERS AND SPECIFICATIONS


CTA-ID : 2024610
Was this helpful?
What can we do to improve the information ?