Technical FAQs

Ask a Question

What is the part number for DC Bus fuse on ATV66C10N4, C13N4, C15N4, C19N4, C23N4, C28N4, C31N4?

There are several different DC bus fuses used in this range of drives. Check the serial number and part number of the drive and select the fuse as shown below:
For all ATV66C23, C28 and C31 drives use VY1ADF400V700.
For ATV66C10N4 and C13N4 where the 7th digit of the serial number is not = 1 use VY1ADF400V700.
For ATV66C15N4 and C19N4 where the 7th digit of the serial number is not = 1 use VY1ADF450V700.
For ATV66C10N4 and C13N4 where the 7th digit of the serial number is = 1 use VY1ADF250V700.
For ATV66C15N4 and C19N4 where the 7th digit of the serial number is = 1 use VY1ADF350V700.
The listed part numbers are for one fuse. Order the correct quantity based on the need.


CTA-ID : 2024657
Was this helpful?
What can we do to improve the information ?