Technical FAQs

Ask a Question

What is the DC Bus voltage trip threshold for ATV31?

Overvoltage Trip
For drives with part numbers ending in M2, M2A, M3, or M3A DC bus voltage overvoltage level is 400 VDC.
For drives with part numbers ending in N4 or N4A the DC bus voltage overvoltage level is 840 VDC.


CTA-ID : 2024469
Was this helpful?
What can we do to improve the information ?