Technical FAQs

Ask a Question

Are there any EZM Branch Devices available with seven meter sockets in one device?

Issue:
Current product design

Product Line:
EZM Metering

Environment:
Number of meter sockets

Cause:
Additional meter sockets

Resolution:
The Current Design EZM Branch Devices DO NOT have more than 6 meter sockets in ONE device. The ONLY Branch devices that contain 6 meter sockets are some of the 125amp branch devices, the 225amp branch devices contain up to 5 meter sockets Max.  A customer would need to obtain multiple EZM branch devices for more than 6 meter sockets.


CTA-ID : 2024594
Was this helpful?
What can we do to improve the information ?