Technical FAQs

Ask a Question

I am using a DJM32400 breaker in an EZML331400 branch device. Can I get a lug to use two conductors at the load side of the breaker? Using 2 4/0 conductors in this application.

The alternate lug kit is catalog number 32510. This is a box of three two barrel lugs with a wire range of 2/0-350 CU 2/0-500 AL.

CTA-ID : 2024593
Was this helpful?
What can we do to improve the information ?