Technical FAQs

Ask a Question

What loading should an NW30H 3000 amp breaker have before the display starts working? The trip unit is version 6.2A.

You will need up to 20% load on the breaker or 24 Vdc on terminals F1 and F2 for the display to start working.

CTA-ID : 2024590
Was this helpful?
What can we do to improve the information ?