Technical FAQs

Ask a Question

Does an MXL36600G breaker need 120V control power to operate the ground fault sensing, or is it for testing only?

The breaker will sense a ground fault without the 120 V control voltage. Application of the 120 V control voltage is for testing purposes only.

CTA-ID : 2024589
Was this helpful?
What can we do to improve the information ?