Technical FAQs

Ask a Question

Can a Main Circuit Breaker Kit be field installed on a QON342L225I OEM Mounting Base?

No, this Main Lug OEM Mounting Base cannot be field converted to a Main Breaker OEM Mounting Base. A main breaker would have to be incorporated into the OEM`s equipment design. The final acceptance of this component is dependent upon its installation and use in complete equipment submitted to Underwriters Laboratories, Inc.

CTA-ID : 2024585
Was this helpful?
What can we do to improve the information ?