Technical FAQs

Ask a Question

What are the repair parts for a QO112M100RB, Series S2(or S02), Load Center?

Current design repair parts

Product Line:
QO Load centers

Repair parts



Only the parts listed below are considered field replaceable.
Cover - 4056317850
Interior Trim with Labels - 4056312801K (remove main KO in the field)
Interior Assembly - QO112M100RBI
Neutral Bonding Screw - 4028345850K
Main Circuit Breaker - QOM100VH
Interior Trim Mounting Screw - 4020513001K
RB Door Mounting Screws - 2142217101
Outdoor Cover Latch - 4056314701
Outdoor Latch Rivet - 2410212160
Main Circuit Breaker and Main Lug Keps Nut - 2342702001

CTA-ID : 2775
Was this helpful?
What can we do to improve the information ?