Technical FAQs

Ask a Question

What is the part number for the adapter included with XCKP106 that goes from metric to 1/2`` NPT?<br /><br />

The XCKP product line does not use an adapter . It has a 1/2 `` NPT molded conduit opening integral in the body .

CTA-ID : 2025032
Was this helpful?
What can we do to improve the information ?