Technical FAQs

Ask a Question

What is the part number for the adapter included with XCKT145 that goes from metric to 1/2`` NPT?<br />

DE9RA1012 is the adapter.


CTA-ID : 2025031
Was this helpful?
What can we do to improve the information ?