Technical FAQs

Ask a Question

How do you order a QO342MQ225 with a QGL or QJL main circuit breaker provided, factory installed, instead of the standard QDL main circuit breaker?

Add a QGL or QJL suffix to the catalog number of the device, ie: QO342MQ225QGL or QO342MQ225QJL.

CTA-ID : 2024562
Was this helpful?
What can we do to improve the information ?