Technical FAQs

Ask a Question

Is there a Class 2511 Type M or Type T reversing manual starter in NEMA 4/4X enclosure?

No, available as open style or NEMA 1 surface mount only.


CTA-ID : 2024560
Was this helpful?
What can we do to improve the information ?