Technical FAQs

Ask a Question

Can you use a PQ4620G to replace a PQ4220G?<br />

Customer can use the PQ4620G. However, the fuse spacing will be set up for 600V fuses, not the 240V fuses. The fuseblocks can be moved to accept 240V fuses, but the nameplate will still read 600V.


CTA-ID : 2025172
Was this helpful?
What can we do to improve the information ?