Technical FAQs

Ask a Question

Is a CU12L400CN UL listed as Suitable for use as Service Equipment?

Yes, it is. This Combination Service Entrance Device is suitable ONLY for use as Service Equipment.


CTA-ID : 2024745
Was this helpful?
What can we do to improve the information ?