Technical FAQs

Ask a Question

How do you order a QO342MQ225RB with a QGL or QJL main circuit breaker factory installed, instead of the standard QDL main circuit breaker?

Add a QGL or QJL suffix to the catalog number of the device, ie: QO342MQ225RBQGL or QO342MQ225RBQJL.


CTA-ID : 2025350
Was this helpful?
What can we do to improve the information ?