Technical FAQs

Ask a Question

Can the 9037 Type EG type float switch be used in diesel fuel?

This switch will function properly in diesel fuel having at least a density of .8. It must fully submerge in order to generate the force to trip the contacts. However, the float will not float in fuel of a lower density such as .6 or .7 and could not function in those thinner fuels

CTA-ID : 2024989
Was this helpful?
What can we do to improve the information ?