Technical FAQs

Ask a Question

Are neutrals available for the J enclosure to provide 200% capacity?<br />

Neutrals can be added to the J enclosures to provide 100 and 200% capacity.
The enclosures will accept the following neutral assemblies: SN100FA & SN400LA.



CTA-ID : 2025130
Was this helpful?
What can we do to improve the information ?