Technical FAQs

Ask a Question

Is the plastic mounting bracket for a Class 9999 Type SA2 Start/Stop control station available or does the complete unit have to be replaced?

The part is available as a replacement item, order 31033-016-01.

CTA-ID : 2024724
Was this helpful?
What can we do to improve the information ?