Technical FAQs

Ask a Question

What is the AIR for HG breakers?

At 240 V they are rated at 65 kA , at 480 V they are rated at 35 kA and at 600 V they are rated at 18 kA


CTA-ID : 2025119
Was this helpful?
What can we do to improve the information ?