Technical FAQs

Ask a Question

What is the max branch breaker that can be installed in a HOM816M200FTRB load center?

The HOM2200BB is the largest branch breaker that will fit into this load center.


CTA-ID : 2025112
Was this helpful?
What can we do to improve the information ?