Technical FAQs

Ask a Question

Will the QBMIK mechanical interlock kit for Powerpact Q frame work with one 2 pole breaker and one 3 pole breaker?

Yes. It will work with the 2 pole breaker on either side of the 3 pole. It will also work with two 2 pole, and two 3 pole breakers. It cannot be used on I-LINE breakers.

CTA-ID : 2024307
Was this helpful?
What can we do to improve the information ?