Technical FAQs

Ask a Question

What is the NEMA rating of the D11SF__ rotary style operating handles for the D10 disconnect switches?

These rotary handle operating mechanisms are rated NEMA Type 1, 3, 3R, 4 and 12 only



CTA-ID : 2024301
Was this helpful?
What can we do to improve the information ?