Technical FAQs

Ask a Question

Is door-n-door construction available in the a NEMA 12 NQOD panelboard?<br /><br /><br />

Yes. It is only available in the following sizes:

29H x 20W x 6.5D
50H x 20W x 6.5D

This is an option in Product Selectors.

CTA-ID : 2024121
Was this helpful?
What can we do to improve the information ?