Technical FAQs

Ask a Question

What is the part number for the 115V I/O extension card for Altivar 66?

The ATV66 Drive became obsolete July 15, 2004. Therefore, the parts may become unavailable in the near future.
There are 2 possibilities:
The VW3A66202T includes AO3 (Analog output 3)
The VW3A66202AT does not include the analog output.
The number VW3A66202 may be printed on the cards. To order, the ``T`` or ``AT`` must be added to the part number.

CTA-ID : 2024118
Was this helpful?
What can we do to improve the information ?